Cancel
Showing results for 
Search instead for 
Did you mean: 

Drop into assembly from windows explorer has quit working

Phenom
Phenom

I prefer to work with open windows folders open so I don't have to navigate all over the place using the parts library flyout in solid edge. I find it easier and have worked this way for as long as I can remember. In an assembly, if I want to add a part I simply find it in my folder, then drag and drop it into the assembly and add relationships and move on. Starting last week this stopped working. It still works if I use the Parts Library, but doesn't work if I drag from windows explorer. When I drop it in, the cursor changes as if it is going to place it, but then it just stays like that with the little + sign. See video I just recorded below. Sorry about the aspect ratio I needed it to show more than one monitor so you could see everything.

(view in My Videos)

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
2 REPLIES

Re: Drop into assembly from windows explorer has quit working

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @nominus38,

 

I work this way [Windows File Explorer] also....and have seen no functionality difference.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Drop into assembly from windows explorer has quit working

Siemens Phenom Siemens Phenom
Siemens Phenom

Working for me with ST10 MP5 and Windows 7 Explorer.

 

Try this under a different Windows User profile... that or just reset your Solid Edge user preferences...