Cancel
Showing results for 
Search instead for 
Did you mean: 

Dual Dimensions for hole callouts

Creator
Creator

I am trying to add dual dimensions to the hole callouts.  I am working in the draft template under styles.  In the example shown in the attached file, I would like to show %HS as a dual dimension, so I click the value, then Format, but when the format values opens it is grayed out and i can't make the necessary changes.  I have tried to manually make the changes using %{%HS/du} but that only gave me the dimension with "/du" as a suffix.  So can anyone tell me where I am going wrong.  Thank you in advance for your time and assistance.

JD Haigler
18 REPLIES 18

Re: Dual Dimensions for hole callouts

Siemens Phenom Siemens Phenom
Siemens Phenom

What version of NX are you using?

There is no dual dimension setting for the hole callout either in Drafting or PMI application.

You can use the appended text as per your need to display the information.

Highlighted

Re: Dual Dimensions for hole callouts

Creator
Creator

I am using Solid Edge ST9. 

JD Haigler

Re: Dual Dimensions for hole callouts

Creator
Creator

Sorry I didn't realize i was posting in an NX forum.

JD Haigler

Re: Dual Dimensions for hole callouts

Siemens Phenom Siemens Phenom
Siemens Phenom

@AmyReyes1: Could you please move this to the SE forum.

Re: Dual Dimensions for hole callouts

AmyReyes1
Retired

Done! Smiley Happy @Shotman77 someone on the Solid Edge forum will be able to answer your question. 

 

Thanks, 

Amy


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Re: Dual Dimensions for hole callouts

Legend
Legend
That doesn't appear to work for annotation of holes which makes some sense as a 1"-8 UNC tapped hole is not the same as a M25 even if they are roughly equiv.

Re: Dual Dimensions for hole callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For tapped holes, sure, but not all holes are tapped.

Anyway, this has already been posted in the SE forum previously so this thread is redundant.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Dual Dimensions for hole callouts

Legend
Legend
Yea I just saw the second thread here for this.

From what I have seen SE treats threads and other Hole features like they are special and not just geometry, c'bore holes etc also behave the same.

Re: Dual Dimensions for hole callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yeah, but shouldn't they (not tapped ones) be able to be dual dimensioned and toleranced too?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200