Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dual Dimensions

Genius
Genius

Hi Guys.

 

I am setting up new styles and for dimensioning I am also setting up a new dual dimension.

The issue I have is the decimal places.

As you can see by the image I have 'RAD DUAL' to zero decimal places and if i want to go to 2 or 3 decimal places I use the dropdown below the standard chosen.

In 'mm' it does change but in 'inches' it doesn't.

How do I get the inches to change like it does in 'mm'

 

Capture.JPG

 

Kind regards

 

Darren.

3 REPLIES 3

Betreff: Dual Dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

 

just click the button besides the main round off button

 

20181024_1123.png

regards
Wolfgang

Betreff: Dual Dimensions

Genius
Genius

Hi Wolfgang.

 

Everything works as I want it to for MM but not for INCH.

 

The advanced round up gives me the same result.

The only way i can show to decimal places is if I change the linear round-up as shown.  I want it to be adjustable like in MM.

 

Capture.JPG

 

Darren

Betreff: Dual Dimensions

Genius
Genius

Hi Wolfgang.

 

I think I mus-understood what you were saying.

 

The advance round-up is the only way to adjust them both together.

 

I like it.

 

Thanks

 

Darren