Cancel
Showing results for 
Search instead for 
Did you mean: 

Duplicate filename error using Inisght API

Creator
Creator

I have a vb.net project for ST9 that moves (renames) asm files from one folder to another on the server.  On occasion, an asm fails to move because it says there are duplicate names found.  I've checked the folders and the file exists only once in the source folder and doesn't exist in the target folder.  My question is two fold.

 

1) Is there a reason I'm getting a duplicate name error that I can't see through Windows Explorer, Design Manager duplicate tool, and sharepoint?

 

2)Is there a way for my project to know that it fails without having the Solid Edge DisplayAlerts active?  I'd like for my program to log the failure and move on without human intervention.

3 REPLIES

Betreff: Duplicate filename error using Inisght API

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Josh_

 

 

maybe it is better to ask that question in the Programmers Forum rather than in this General forum.

There obviously will be more people able to answer Your question.

 

 

regards
Wolfgang
Highlighted

Betreff: Duplicate filename error using Inisght API

Creator
Creator

Thanks for the help.  I'm new here and was unaware of the other forums.

Re: Duplicate filename error using Inisght API

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If it's a managed system like Insight, SESP, Teamcenter, etc. it likely won't allow duplicate filenames anywhere in the database.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200