Cancel
Showing results for 
Search instead for 
Did you mean: 

ER 7851802 - Bend lines with angle information

Legend
Legend

Good day everyone, with this topic I would like to see if we are the only one with this reqeust. Also if possible I would like to gather as much support from the community as I can get ofcource. This case is 1 out of 2 of our biggest wishes in our wishlist in Solid Edge.

 1 Gpi logo.png

 

Company: GPI

Website: www.gpi.nl

 

System:

Windows 10 Professional

Solid EdgeST8 – MP12

 

Solid Edge seats:

GPI – Division Netherlands:  11 Seats.

GPI – Division Poland:  5 Seats.

 

Our product contains an 100% custom made dynamic environment in Solid Edge.

 

2 Gpi uitleg.PNG

Problem case

For this problem I took an project that was easy to compare. These two projects have the most resemblances with each other, to have the best case with improving lofted flange.

 

Solid Edge:

3 Solid edge tekening.png

 

 

Autocad:

4 Autocad tekening.png

 

Solid Edge: Lofted flange flatten with bend table.

5 Solid edge bend table.png

Autocad: Produced cone from an lisp that gave the bending line and angle.

6 Autocad bend uitslag.PNG

 

The lisp has been made approx 15years ago, and till today SE doesn't provide any information about bending lines within the lofted flange.

 

I have tested it in ST10, and because of that I now would like some opinions from the community.

Sander
The Netherlands
5 REPLIES 5

Re: ER 7851802 - Bend lines with angle information

Gears Phenom Gears Phenom
Gears Phenom

Hi Edgers,

 

Just wondering would anyone help me to find the way how to add the bendline angles to the flat drawing ?

 

as @Sander-NL mentioned, the bend table tells only about 2 sequences (1 and 2 one the drawing ).

 

Thank you

 

bend lines angle.png

 

Highlighted

Re: ER 7851802 - Bend lines with angle information

Valued Contributor
Valued Contributor

Will this callout work? Capture.JPG

Re: ER 7851802 - Bend lines with angle information

Gears Phenom Gears Phenom
Gears Phenom

Hi @Milro

 

Fantastic job.

 

I've forgotten about it - nice Trick !!

 

Thank you,

 

Arek

Re: ER 7851802 - Bend lines with angle information

Legend
Legend

@Milro

 

The only thing is that practical 4 times 22degr is wrong with bends from square to round. Man Wink.

Sander
The Netherlands

Re: ER 7851802 - Bend lines with angle information

Valued Contributor
Valued Contributor

You are right , I don't do a lot of completely square to round  mostly round to round .Sometimes flat to round 

which will give me a Lofted Flange : No Data error do to the fact that the angle will change 

from one end of the bend to the other . I agree that it would be nice to have a more robust solution

to lofted flange bend info.