Cancel
Showing results for 
Search instead for 
Did you mean: 

ER Edges of part used to stack dimension

Legend
Legend

Wouldn’t it be nice if the edges of a part could be used to stack the dimension.

 

See attached video

 

I have put a "hidden" dimension on the edge in order to show this desired behaviour in a drawing.

 

Kind Regards,

 

Jan Bos

Manager R&D/Engineering

Geha, The Netherlands

(view in My Videos)

 

5 REPLIES 5

Re: ER Edges of part used to stack dimension

Gears Phenom Gears Phenom
Gears Phenom
I would love such a function.
If you open an ER please provide it so I could add my vote.

Francesco

Re: ER Edges of part used to stack dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm missing what the problem behavior is and what the desired behavior is.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: ER Edges of part used to stack dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jan_Bos

 

 

 

maybe the function "Align Dimensions" 20161207_2033.PNG can help You a little.

It is not exactly what You were asking for but at least with ST9 You can define a certain distance from edge of geometry to be away together with the standard stack distance from dim to dim

 

 

regards
Wolfgang

Re: ER Edges of part used to stack dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand wrote:

I'm missing what the problem behavior is and what the desired behavior is.


Hi Bruce,

 

As I understand it....Jan would like to get the "inferred stack" alignment indicator to appear for the 'second" [alternate placement] dimension, not just the ones stacked on the base dim. Sort of like how ordinate dims continue the previous dim placement setting.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ER Edges of part used to stack dimension

Legend
Legend

Bruce,

 

There is no problem, it's an ER.

 

Look at the placing of the 43 dimension. I hoover over the edge and there is no dotted line appearing for stacking this dimension at 10mm from the edge..

 

By placing the other two dimensions I hoover over the edge and this dotted line appeas and I can stack the dimension. (I have hidden a dimension on the edge, just for the purpose of this video)

 

This would be nice to have in ST11, stacking dimensions will start on 10mm (Iso) or 18, 24, 30, 38, etc.

 

Kind Regards,

 

 

Jan Bos

The Netherlands