Cancel
Showing results for 
Search instead for 
Did you mean: 

ERA Rotate

Pioneer
Pioneer

I am trying to create a view of a case within ERA that show it open and closed but when I go about rotating the lid it only rotated around the xyz coordnate and not the hinge.

4 REPLIES

Betreff: ERA Rotate

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @lostriver319

 

 

not being able to fully understand and imagine Your situation, I think, that if You define a variable motor for the angular relation in assembly, You should easily be able to animate it via ERA.

 

 

regards
Wolfgang

Re: ERA Rotate

Valued Contributor
Valued Contributor

If you are using the drag component command to rotate the part, you can click "Orient Triad From Geometry" to select the hinge you want to rotate about.

Re: ERA Rotate

Pioneer
Pioneer

I tried that and it keeps going back to the org xyz cord

Re: ERA Rotate

Gears Phenom Gears Phenom
Gears Phenom

maybe underconstrained components?

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7