Cancel
Showing results for 
Search instead for 
Did you mean: 

EROR WHILE SAVING A PART FILE IN TO STEP FILE

HI eror.PNG

 

Please find the attached error while save as the part file into step file ... ,

i wanted to save as  this part file into step file again . but im unbale to do this operation . please help me out.

 

Thank you

Preetham

7 REPLIES 7

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there @PreethamGowda,

This is because you have a model that has no "Solid Bodies".....it appears to be all construction surfaces. Presumably this is an imported part/assembly file.
I'm not at a PC right now, so can't verify the process....but, you might look at the "Options" during the Save As (STEP) to include constructions.
Alternatively interrogate and repair the file to become a solid model....by closing the surfaces if gaps are present, then stitch them should make it a solid.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

Hi Sean

Thanks for your reply to my problem,

i checked with the "option" while saving it to STEP file . even i include Construction still i'm not able to save .
please find the below attachement for your refrence .

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

hi Sean

 

can you help me out how to identify the gaps in the surface and make it to solid body .

 

Thank you

Preetham

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

error2.PNG

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PreethamGowda 

 

 

turn on the second construction options (sheets)

 

I suppose Your geometry is not building a closed solid (this is what closed means too) body.

So with activated sheets they should be exported too.

regards
Wolfgang

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @PreethamGowda,

 

Sorry for the delay. I replied to your post at midnight, and really shouldn't have been awake. Robot Indifferent

 

Something else you might consider, "if this is an imported part"......try opening it into your Assembly template. Depending on how this part was modelled, it should [hopefully] make all the parts solid models, in their own right.......making it far easier to work with.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: EROR WHILE SAVING A PART FILE IN TO STEP FILE

Hi Sean

 

Thanks for your support .

 

Preetham