10-12-2017 05:57 AM
Hi Edgers,
I am looking for a way where I could create a button or a shortcut for a Edit Formula command.
I couldn't find this command within All Comands to add/modify a Quick Access Toolbar.
any idea how to do it ?
It is annoying me to click 3-4 times to add new variable - This should be able to do within the box Select-Dimension Value or quicker way.
thanks
Arek
Solved! Go to Solution.
10-12-2017 08:45 AM
10-12-2017 08:47 AM
Hi @arekkul
or if You are talking about a new customer variable (and not a formular for a dimension) then open the variable table and enter it there into the last line
Tip: on every machine I ever have setted up for SE there YOu will find the shortcut Alt-V to enter the varaible table
Simple, easy and fast
10-12-2017 08:54 AM
I've been wondering about this too. IMO SE is clumbsy with doing variables in the modeling environment. If I want to make the variable i'm placing/editing equal to another variable I should be able to just double click that variable and be done. If I want some function I can start typing, then double click the other variable to insert it and then finish typing the formula. This idea of haveing two entry modes on a dimension, one for numbers and another environment for formuli is just something I've learned to live with. So if someone has a suggestion or there's a checkbox in some menu some where I too would be greatful to hear about it.
10-12-2017 08:58 AM
Hi @hawcad
The Double click the dimension option is very useful - never heard of this before.
thank you.
this will help for a while ...
cheers,
Arek
10-12-2017 09:01 AM
Hi @bnemec
can You better explain what the goal should be?
If I double-clik a dimension, I automatically enter the formula mode.
So from here You can enter any formular into the formular field and You can single-click any other dimension to be placed witihn that formular filed.
Is this what You are looking for?
10-12-2017 09:04 AM - edited 10-12-2017 09:11 AM
@hawcad, the keyboard shortcut to the variable table is helpful. I would have to disagree that it is simple easy or fast. I find it powerful. I'm venturing a guess that some difference comes here in modeling style and previous CAD softwares that we get used to. If someone is doing a fair bit of geometry in sketches, either for skeletal layout or just complicated parts, bouncing back and forth between variable table and the sketch is clumsy. Imagine if editing a dim was a bit like in excel, where you just select some other variable when you want to insert it.
Edit: we must be typing at the same time.
What I'm saying is the formula entering mode is a waste of time, I cannot (or don't know how) to get to it without leaving the dimensioning mode then double click as you say to get the formula mode. If I'm editing a dimension value, say typing in some number, I should just be able to double click some other dimension and it will paste that variable name into the editing box I'm in. That is what I was used to and it is simple and fast, the variable rules and formula helper was part of the create dim command.
10-12-2017 09:12 AM - edited 10-12-2017 09:14 AM
If you have the variable table open and you edit formula of a dimension in addition to being able to select another dimension you can cut and paste variable names and formulas from the variable table into the formula box.
But it's true there is no formula helper that is with the dimension itself.
10-12-2017 09:19 AM
So @bnemec
this is where the Double-Click come into the play.
See video and I hope it helps
10-12-2017 12:26 PM
As @hawcad says --> Double Click is the WAY.
Also, don't forget you can click on other dimensions when building the formula in the little dialog that pops up. This too is key -- you don't have to know their variable names.