Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Edit Formula Command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

how was it possible to forget this one?

 

Ash onto my head!

 

regards
Wolfgang

Betreff: Edit Formula Command

Phenom
Phenom

@hawcad  did you forget the <sarc> </sarc> tags?  Smiley Happy

 

I'm with you though.  Is there a wall hanging or poster with this stuff on it?  No way my brain can retain all these tips, tricks and functions.


If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.

Betreff: Edit Formula Command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad  Funny thing is I tried that on a Dimension I just placed and it did not work.  Tried it again and couldn't get it to work until I modified the dimensions value, after which I can double click the dimension lines and can get the formula bar.

 

Out of this little exercise it should be obvious that command consistency is very important, especially when you have the same command that exhibits different user interaction behaviour between Sketch and PMI modes. (@AdityaG)



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Edit Formula Command

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@KennyG

Not seeing it here with ST8 - the former part of your comment about first modifying the PMI vaule to enable fomula editing.

But in full agreement with the later part, glad to see someone breaking the ice on this topic about consistency

@Rahul_Kulkarni@SandeepM@ksbhadekar@dcstaples

 @Rahulk