Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit dimensions in draft file

Pioneer
Pioneer
Hello there,

I was wondering, can the dimension changed in draft file format without have to go back in tp part assembly file. ? If yes, please guid me.
4 REPLIES 4

Re: Edit dimensions in draft file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Dimensions can be over ridden in Draft, but they cannot change the model.  If you need to update the model, double click on your drawing view which will open the model, make the change, and then close and return to the Draft and update the views.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Edit dimensions in draft file

Creator
Creator

how to override the dimension?

Re: Edit dimensions in draft file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How to override a dimension:

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
Highlighted

Re: Edit dimensions in draft file

Phenom
Phenom

You don't really even need to go to the trouble of hiding the dimension and using the prefix/suffix. You can simply click on the dimension value and change it to whatever you want it to be. This, by default, will place a line under the dimension indicating that it is no longer to scale. The "not to scale" underline can be modified or turned off completely under properties if you so desire.

 

That said, just because you can to do this, doesn't mean you should do it. In my group, changing a dimension like this on a production drawing rather than editing the model and making the dimension correct would constitute a hanging offense.

 

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317