Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Editing sweep protrusions (ordered)?

Valued Contributor
Valued Contributor

I'm trying to edit the profile of a sweep protrusion (ordered environment) but am stuck.  If I go into the definition and select the profile step, I'm asked to "select a path or cross section to edit".  If I select the cross section (there's only one) it turns green, but nothing more happens.  It doesn't reorient the window to the profile plane or show any of the 2D editing tools like it did when I first created it.  Hitting the edit button doesn't appear to do anything either.  What am I missing?

 

Thanks

Pat 

6 REPLIES 6

Re: Editing sweep protrusions (ordered)?

Pat,

 

Is your profile driven from a global sketch?

ie:  is the sketch visable in the path finder?

if so you just edit the sketch directly.

 

if the sketch is feature based then you need to use the edit profile option:

http://screencast.com/t/D5hALsAn03ti

 

 

Re: Editing sweep protrusions (ordered)?

Valued Contributor
Valued Contributor

No, the profile was created directly in the command (like I do with most features).  I expected edits to work the same way as it does with other commands, where it takes you back into the same sketch environment you used to create the profile originally.  That would be logical as least.  Not sure why it's different here, unless there's a bug in the software (I'm still on ST7).

Re: Editing sweep protrusions (ordered)?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you watch Matt's video?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Editing sweep protrusions (ordered)?

SEE THE VIDEO... YOU NEED TO RE ENTER THE PROFILE...

 

http://screencast.com/t/D5hALsAn03ti

Re: Editing sweep protrusions (ordered)?

Valued Contributor
Valued Contributor

Opps!  Sorry Matt.  I didn't look at your video (thought it was sketched based).  But that solved the problem.  I didn't realize I needed to click on the "Sweep Protrusion - Draw Profile Step" button.  That was step I was missing.  Glad it turned out to be something simple.  Thanks!

 

 

Re: Editing sweep protrusions (ordered)?

Phenom
Phenom

Editing sweeps and lofts can be a bit of a challenge, so I always create the profiles as seperate sketches, not as part of the feature.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.