Cancel
Showing results for 
Search instead for 
Did you mean: 

Eliminating Ribs In Loft

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

With This Video I Have A Part That Is In Loft Command... Needs The Ribs Eliminated From The Drawing

Any Thoughts?

 

Thank You

GregoryLee

 

http://screencast.com/t/6r9p254pTewz

 

 

1 REPLY

Re: Eliminating Ribs In Loft

MLombard
Retired

I'm going to guess that those edges have something to do with the cutouts. It's hard to tell without the part file. If you delete or undo the cutouts, those ridges will probably go away. Not sure what you're trying to accomplish here. Maybe a Thin Wall feature will help.

 

Also, I'd probably suggest that you make things like loft features in Ordered. I usually suggest people try Synchronous, but for features like the loft, they can't be edited in Synchronous.

 

One cool thing you can do is put the sketches in Synchronous with the Loft in Ordered.

Retired Community Manager for Solid Edge. This account is no longer active.