Cancel
Showing results for 
Search instead for 
Did you mean: 

Embossed Pattern

Pioneer
Pioneer

Hi all

 

I am trying to make a chequered plate with embosed pattern on it.

I can emboss a single feature and patterenize it but this would lead to a very heavy file and for steps would become slower.

Is there any way to patteronize any object and the handling remains faster.

 

Basically I do want to show that pattern in draft. Can texturing feature could help me..??

or texturing only refers to graphical representation which has nothing to do with drafting..

 

see attached file for sample sheet

7 REPLIES

Re: Embossed Pattern

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi:

 

See the third video in this tip.

Or as below:

 

 

Hope this gives you a hint.

 

~Tushar Suradkar

 

Re: Embossed Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Further to to what @Tushar shows.....if you show your model as shaded in draft, the applied texture will also show there. [see attached PDF]

 

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Embossed Pattern

Pioneer
Pioneer

thanks for your suggestions.

But what I an asking is that is there any way to show details of this "textured pattern" in draft.I mean to say that I want to show height and width of that pattern.

What I do know that it is not possible. But I have not much experince as you guys have.

 

 

 

Re: Embossed Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@AM2 wrote:

I mean to say that I want to show height and width of that pattern.

What I do know that it is not possible. But I have not much experince as you guys have.


 

Hi there,

 

You can do this also....just model the ridges and pattern them on the flat sheet metal file, then re-bend, or apply new bends, and they will flatten.

 

ST8_PSM_ChequerPlate[1].png

 

ST8_PSM_ChequerPlate[2].png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Embossed Pattern

Pioneer
Pioneer

Thanks for your informative reply.

I have a question that by following your procedure, will it make my file heavier..??

as I have to deal with large assembly file

Re: Embossed Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Any time you add faces files become more computationally intensive. You can simplify parts and assemblies to lessen their downstream impact.

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: Embossed Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @AM2,

 

Yes, as @bshand points out....adding additional detail, creates a scalar tax on your system, but this can be managed, as Bruce also says, with using simplified models, for use in larger assemblies.....a trade off, for having to have such details usable downstream.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000