Cancel
Showing results for 
Search instead for 
Did you mean: 

Error In Feature Library

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Good Morning Everyone,

 

I saved a doc. in save as, Go to the file and comes up with an error in the feature library and will not load in the sync. par. doc..

 

http://screencast.com/t/7ZQUdhULI5US

 

Than You

Greg

1 REPLY
Highlighted

Greg, as far as I know, the feature library is not meant...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg, as far as I know, the feature library is not meant to be used to create initial geometry, it is only meant to capture features of existing geometry and apply them to other existing geometry.  http://support.industrysoftware.automation.siemens.com/training/se/106/en_US/en_US/selfPacedExt/spse...



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com