Cancel
Showing results for 
Search instead for 
Did you mean: 

Error On Using Circle and Line

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Thank you for the download for the ST10.

I have an issue with applying a circle and a line on an ASNI part.

While applying circle and a line... to me I'm getting a reverberating effect.

I've looked at all commands, I can not find anything that is on.

Is this something that is on ST10?

I have an attachment to show the problem 

https://www.screencast.com/t/jQWunsrn

How can I fix this problem

Thanks

Greg

 

 

 

 

3 REPLIES 3

Betreff: Error On Using Circle and Line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @PO_LC

 

 

so this simply has nothing to do with circle or line this just is a graphics card issue, regarding driver versions and/or settings.

 

See another posts with graphics problems and follow that hints.

 

Let us know which OP and graphics card You are using, make a search here for graphic issues and You finally (hope so) will be successsful

 

regards
Wolfgang

Re: Error On Using Circle and Line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@PO_LC,

 

Good grief, that is terrible graphics performance......I thought you purchased a BOXX computer to run Solid Edge on, way back. I would be looking as system settings as the main issue here, and as @hawcad says, it is most likely a graphics [driver] problem. Make sure you have all possible [compatible] system updates installed.

 

This was your post from 2014....

https://community.plm.automation.siemens.com/siemensplm/board/message?board.id=Solid-Edge-Student-Ed... ....do you still have this system?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Error On Using Circle and Line

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

The Boxx computer has been down for about for about year. I've been using my laptop.

This is one of the reasons I've been using ST8. 

Since ST10 has been out for a while... I wanted to upgrade, not knowing that this laptop cannot handle the workload.

I've been in touch with Boxx Computer for more power.

 

Thanks

Greg