Cancel
Showing results for 
Search instead for 
Did you mean: 

Error message: application environment cannot be started

Hello,

yesterday I bought a new laptop (hp omen 15 dc 0003) nad firstly I updated Windows and drivers... after updates, I wanted to install my education version of SE 2019 the installation was successful but I got an error message after start (application environment cannot be started). I do not know how can I solve this error now. I tried to reinstall the program but it is not the solution.

Please if you had an error like this help me out somehow. Thank you for your answer.

2 REPLIES 2

Re: Error message: application environment cannot be started

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imrich_Miller Guessing Windows 10 updated to version 1903 and you are running AVG or Avast for anti-virus?

 

Removing your anti-virus and using Windows Defender anti-virus will allow Solid Edge to run.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Error message: application environment cannot be started

@KennyG Thank you for your fast answer! Yeah that update... and antivirus too.

 

After removing Avast the message is disappeared too. (disable option is not enough).