Cancel
Showing results for 
Search instead for 
Did you mean: 

Error message when right clicking to launch Design Manager.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi everyone,

I have following problems:

 

When try to right click on a file and "open in design manager" I get an error message stating "there was a problem sending the command to the program"

Someone managed to solve this problem ???

2 REPLIES

Re: Error message when right clicking to launch Design Manager.

Gears Phenom Gears Phenom
Gears Phenom

Good morning,

 

I am experiencing this problem as well.  I submitted an IR on this problem.  The issue is related to the software architecture and a fix will not be in place until ST10.  My solution is to put a Design Manager shortcut on the tool bar at the bottom of the Windows screen.  Not very convenient when trying to revised models etc. but for now it's the only choice.  I'll look up my post and send you a link.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Error message when right clicking to launch Design Manager.

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

Here is a link to the thread along with the IR number:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/ST9-Problems-with-Design-Manager/m-...

 

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1