Cancel
Showing results for 
Search instead for 
Did you mean: 

Errors when opening solid edge

N/A

Hello,
I've got email after registration. Downloaded the installer and license file.
After that I installed Solid Edge as a administrator.
When I try to open Solid Edge I've screens like this(set back clock issue):


My clock in windows and in bios is set to today date(after that i tried the further date one month, year and it hasn't worked).
I also tried to reinstall with cleaning the regitry.
In the license file I've got on the first line date 1-mar-2014.

My computer:
Asus VX6
1,8 GHz Dual Core
4 GB Ram
Windows 7 Home Premium.

Do anyone know how to solve this problem?

Thanks for reply.

Greetings,
Wiktor.

5 REPLIES

Re: Errors when opening solid edge

Siemens Phenom Siemens Phenom
Siemens Phenom
Wiktor,
Based on your screen shots it appears that you have hide known file
extension enabled in Windows Explorer. More than likely your
SELicense.dat file has been incorrectly named to SELicense.dat.txt
In Windows Explorer disable hiding file extensions and rename the file
back to just SELicense.dat.
Regards,
-Dave

On 20/02/2013 14:01, wiktorkrzeszewski@gmail.com wrote:
>
> Hello,
> I've got email after registration. Downloaded the installer and license
> file.
> After that I installed Solid Edge as a administrator.
> When I try to open Solid Edge I've screens like this(set back clock
> issue):
> >http://i48.tinypic.com/wv2901.png]
> >http://i45.tinypic.com/34t75mo.png]
> My clock in windows and in bios is set to today date(after that i tried
> the further date one month, year and it hasn't worked).
> I also tried to reinstall with cleaning the regitry.
> In the license file I've got on the first line date 1-mar-2014.
>
> My computer:
> Asus VX6
> 1,8 GHz Dual Core
> 4 GB Ram
> Windows 7 Home Premium.
>
> Do anyone know how to solve this problem?
>
> Thanks for reply.
>
> Greetings,
> Wiktor.
>
>

Re: Errors when opening solid edge

N/A
Well,
Before I've written here I checked twice this file. Checked one more time and the same problem when starting Solid Edge.
On the printscreen the file looked like notepad file because its exstension was fixed to be opened by notepad, now fixed this issue and still SE is not working.
Do You have some ideas how to fix the problem with the time?
Greetings,
Wiktor

Re: Errors when opening solid edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
This error can occur if you have any file on your pc with a modified/create date greater than today as the license manager checks that to insure you aren't trying to set the clock back. Perform a search on all your files using a filter of the modified date > TODAY.


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Errors when opening solid edge

N/A
I am experiencing the exact errors upon program startup:
Vista 64 bit
Gateway
4 GB Ram
Has anyone found the solution?

Re: Errors when opening solid edge

N/A
I am also with the same problems, my file was so SELicense.dat SELicense.txt, the renamed and nothing remains to astensao txt.
if someone can help me I am awaiting.