Cancel
Showing results for 
Search instead for 
Did you mean: 

Explode a single part file

Valued Contributor
Valued Contributor

Hi,

 

In  some cases I will design in part edit environment using multiple design bodies rather than creating multiple separate part files and arranging in an assembly file. I only do this in certain cases where it seems simpler and faster. However, I've discovered that you can't use ERA explode tools on a single part file.  Does anyone know if there's a work around or any way to explode a single part file with multiple design bodies? I need to show an exploded view in Draft.

 

Thanks,

 

Matt

2 REPLIES 2

Re: Explode a single part file

Phenom
Phenom

You can publish the multibody which will automatically create a linked assembly and parts with minimal effort. It will, of course, create additional linked part and assembly files, but the resulting assembly can be exploded as normal.

 

I am not aware of an easier way to do it with only the multibody part file itself.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Explode a single part file

Valued Contributor
Valued Contributor
Thanks Bob, haven't published in a while, forgot about it.