Cancel
Showing results for 
Search instead for 
Did you mean: 

Export a single .dft sheet to dxf

Pioneer
Pioneer

I am trying to export a single sheet from a .dft file with multiple sheets, to a .dxf file so I can send it to a vendor without giving unrelated design information. I can't seem to find the option that allows me to export just the one sheet. I thought this was possible in the past?

 

thanks!

 

John

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8
11 REPLIES 11

Re: Export a single .dft sheet to dxf

Legend
Legend

ST8

 

Capture.PNG

Re: Export a single .dft sheet to dxf

Pioneer
Pioneer

Yeah... it seems to be gone in ST9. Not sure what happened. Maybe it's just the user!

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Export a single .dft sheet to dxf

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi i just tried in ST10 in step "2" it is there....

 

 

Re: Export a single .dft sheet to dxf

Pioneer
Pioneer

Thanks for checking this out.

 

Just to walk through the steps:

 

1) I am start in the draft environment on the sheet I wish to translate,

2) go to the "save as" menu and "save as translated"

3) At this point I don't see the same menu as you so I believe I am not using the correct commands. 

 

Thanks,

 

John

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Export a single .dft sheet to dxf

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

You should click on the left side in the Save as translated dialog "Options"

Re: Export a single .dft sheet to dxf

Pioneer
Pioneer

Just as a further point, if I click on the options, I don't get the translation wizard popup menu. So that's leading me to believe I'm going down the wrong path.

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Export a single .dft sheet to dxf

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What happens when you click on the options button?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Export a single .dft sheet to dxf

Legend
Legend

Save As, then set file type to .dxf, then pick options

Re: Export a single .dft sheet to dxf

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Do you use an laptop?

 

Sometimes it can happen, that the dialogs are hidden or on an Screen which is not connected anymore.

 

Try this out:

 

- shutdown Solid Edge

- run regedit

- expand HKCU\Software\Unigraphics\Solutions\Solid Edge\Version 100\UI
- delete this "UI" node
restart Solid Edge