Cancel
Showing results for 
Search instead for 
Did you mean: 

Export file for the Cura Software

Pioneer
Pioneer

Good afternoon.

I would like to help me the next.
Make an object in Solid Edge with certain measures, however, when I export for the Cura Software, it is a very small size.

How do I get it opens in Healing with the actual size? 

 

Thanks,

Jorge Ferreira

1 REPLY

Re: Export file for the Cura Software

Genius
Genius

Jorge,

 

Do you use metric or inch templates ?

I think it is a multiply factor error. I think you have to relook the STL settings for importing or exporting STL files. Mostly it is 25.4 to small or to big...

Or maybe you need to adjust a scale setting in Cura.

 

Just guessing

 

 

Dirk Rutten

Solid Edge STX user