Cancel
Showing results for 
Search instead for 
Did you mean: 

Export transformation matrix oof a assemblied part

Creator
Creator

Hello all,

 

I can display the coordinate informations of an assemblied part under the "Occurrence Properties". But it is not in a matrix form.

 

Is it posible and how is it possible to extract the coordinate information from a part as a transformation matrix?

 

Best regards

Stefan

3 REPLIES

Re: Export transformation matrix oof a assemblied part

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

You will get the Matrix only via the API

 

Solid Edge Assembly Type Library > SubOccurrence Object : GetMatrix Method 

 

Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements

 

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: Export transformation matrix oof a assemblied part

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

SaveAs>PLMXML is another way

LMGi
www.TLMGi.com

Re: Export transformation matrix oof a assemblied part

Creator
Creator

Thank you very much.