Cancel
Showing results for 
Search instead for 
Did you mean: 

Expose Custom Material Property

Creator
Creator

We are using ST8 and would like to expose custom material properties for use on our drafts.  Custom properties are shown below.  Is this possible in ST8?

 

Solid Edge Material Table.png

 

 

I can see other material properties, such as yeild stress.

 

Callout Properties.png

 

Thanks for your help.

11 REPLIES 11

Re: Expose Custom Material Property

Gears Phenom Gears Phenom
Gears Phenom

Im running ST9 MP6 and this appears to work as expected?

6-13-2017 9-53-55 AM.png

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Expose Custom Material Property

Creator
Creator

OK, thanks for the confimation Matt.  Maybe it is just not supported in ST8.  I am running 108.00.08.004 (MP8?).  If anyone knows how to do this in ST8, please advise.

Re: Expose Custom Material Property

Siemens Genius Siemens Genius
Siemens Genius

yes, working as well in ST8calloutproperties.jpgcalloutproperties1.jpg

Re: Expose Custom Material Property

Creator
Creator

Great.  Thank you.

Betreff: Expose Custom Material Property

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi to all,

 

IMHO there is only one other issue concerning the same area.

You are not able to see those custom material proeprties in the variable table.

This is something I would like very very much and hope that it will be implemented asap

 

If there is somebody having ST10 (beta) running) maybe You can test this.

 

 

regards
Wolfgang

Betreff: Expose Custom Material Property

Creator
Creator

Yes. I too would like custom material properties in the variable table to expose them for upload to TeamCenter.

Betreff: Expose Custom Material Property

Experimenter
Experimenter

Hello @hawcad,

 

Thank you for all your support to the community. My team mate Aslam had some great information from you for our team.

We are looking to add custom properties that will act as default physical properties.

Physical Property Manager Inside Assembly show some Material Physical Property. There are some additional properties named with 11,12....can be found in format column.

Is there any way of adding new property here? Like propseed.txt or other templete file.

 

Thank you for your time.

 

Phy Prop Manager-1.jpgPhy Prop Manager1

Phy Prop Manager-2.jpg

Betreff: Expose Custom Material Property

Valued Contributor
Valued Contributor
Hello @Tushar,

Can you please check the above post from our teammate @Shihab_Shahriar?
The issue is very important!
It will be a great help.

Regards,
Aslam

Betreff: Expose Custom Material Property

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Sorry, buddy. No idea.

I too have to wait for @hawcad  or some other expert to chime in.