Cancel
Showing results for 
Search instead for 
Did you mean: 

Express Route

Creator
Creator

Is there a way to create square tubing in express route rather than just the default round tubing?  As with copper, the path will be on different "planes" and not just at a 90° plane.

2 REPLIES

Re: Express Route

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do not believe so.  You will probably need to use Frames, or just create parts using the 3D Sketch function.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Express Route

I have never found this option.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10