Extend to edge command

Pioneer
Pioneer

I cannot find this command in ST8. The help file talks about it but I do not see the icon on the ribbon. I attached a screenshot of my ribbon and the help file.

 

https://docs.plm.automation.siemens.com/tdoc/se/108/help/#uid:extnxt1h

 

I am in a draft drawing if that makes any difference. Help says Is under Sketching tab - Draw group, but I do not see the icon mentioned in the help file. I desperately need this command! Can someone post a screenshot to show me where this is supposed to be located?

1 REPLY

Re: Extend to edge command

Esteemed Contributor
Esteemed Contributor

Extend to Next...  And you may try using the Command Finder in the lower right of screen in the Status Bar.

 

2017-04-05_14-37-29.png


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3