Cancel
Showing results for 
Search instead for 
Did you mean: 

Extraction failure

N/A
After downloading the .exe file and double clicking on the icon, the extractor starts but when it gets to 66% it stops and gives the following message "Extraction Failed, cannot open output file"
4 REPLIES

Re: Extraction failure

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
I can only guess the EXE got corrupted during download. I've seen this in one other case, but that isues was where the user extracted the files from the download and tried moving them around--something got corrupt during the move.

Let me know if you need a new download link and I'll send one along. I'm also asking some others for any ideas on how to address this.

This is an odd issue though.
Kris Kasprzak

Re: Extraction failure

N/A
I downloaded the file again and I get the same error message.

Re: Extraction failure

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
Dang....

Let me get with our support team to see if they have any suggestions. In the meantime, can you send some specifics? Operating system, RAM, hardware specs?

Sorry for the issues, this is a strange one.
Kris Kasprzak

Re: Extraction failure

N/A
I am having this same issue. Was there ever a resolution to this problem? I would prefer a 64 bit download if one was available. Thanks!