Extrude Removing Circular Pattern

Pioneer
Pioneer

I have a tubular item with a circle pattern applied around the edge. I want to cut it into two halves so that I can print it. I've made two copies and eliminating the right half on one copy and the left half on the second copy. 

 

However when I extrude subtract one half it is removing the circluar pattern on the half that is remaining. Is there a setting I can change so it won't do this? 

 

Thanks.

1 REPLY

Re: Extrude Removing Circular Pattern

Esteemed Contributor
Esteemed Contributor

Hi Garnet,

 

Any chance you could share your file here?

 

EDIT: .....maybe you could try using the split command to divide the tube into two "multi-body" parts.

[see attched - ST7 synch model]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000