Cancel
Showing results for 
Search instead for 
Did you mean: 

Extrude shows difference of name in pathfinder as protusion. Why?

Experimenter
Experimenter
 
3 REPLIES

Hi,   Maybe somebody has renamed it (if you didn't do it)...

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Maybe somebody has renamed it (if you didn't do it)... You can rename it for "original name" if you select the feature RMB Rename or F2 and Delete the name and Enter...

 

BR,

Imics

Imics
http://solidedgest.wordpress.com/

Re: Hi, Maybe somebody has renamed it (if you didn't do it)...

Experimenter
Experimenter

extrude protusion.pngHi

No,I didnt rename it ,and neither somebody.When I extrude any closed profile,it shows extrude name as protusion in pathfinder

Re: Hi,   Maybe somebody has renamed it (if you didn't do it)...

Phenom
Phenom
That's because it IS a protrusion. You are "extruding" it. Extrude is the method. Protrusion is the result.
-Dylan Gondyke