Cancel
Showing results for 
Search instead for 
Did you mean: 

Extrusion Problem

N/A

Hi guys,

I have a boring problem:-(

I can do extrusions only in the duplex way.

I can't do an Extrusion in only one direction.

Is there a Trick?

Greetings Georg

3 REPLIES

Re: Extrusion Problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I can't do an Extrusion in only one direction.
Is there a Trick?


Hi Georg, try clicking on the extent direction while still in the extrude command action, located as shown in the this image...

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Extrusion Problem

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Press the Shift key. It should toglle between single and double extent directions.

Re: Extrusion Problem

N/A
Okay thanks i'll try it....

yes it works :-)

THANKS