Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Extrusion problem

Creator
Creator

Checked the pathfinder option - it's already on as per picture.

 

Re: Extrusion problem

Creator
Creator

If it helps me get this done - here is a copy of the files I am working on.

Re: Extrusion problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is what I see and my reference to Pathfinder is the tree on the left of the screen.  You can turn display of object on/off by using the checkboxes.

2016-10-24_11-31-00.png



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Extrusion problem

Creator
Creator

Okay there is something odd going on - the following images are the image of the part as it is loaded, followed by the image of the part if I go into edit mode.

 

You appear to be seeing all the bits related to edit mode but without the edit mode red X something must be setup incorrectly on my setup - Either that or I am doing something horrendously wrong.

 

Re: Extrusion problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK, got it.  Always best to show the entire application.  You are in the assembly.  SE by default hides construction surfaces on all components.  To show them, right mouse click on the part either in Pathfinder or on the screen and then select "Show/Hide Component...".  On the Show/Hide Component form find the "Surfaces" line and put a check in the "On" column.

2016-10-24_14-22-26.png

2016-10-24_14-22-46.png

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Extrusion problem

Creator
Creator

Thank you so much - that certainly makes life easier.

Re: Extrusion problem

Pioneer
Pioneer

Having taught myself all of the mid-major CAD platforms (SE, SW, Inventor) I can attest - there's always a way to make life easier.