Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Eyedropper?

Jason,

 

I had issue too, 

 

I downloaded the source code, added references and used the SE Interop Nuget Package, recomiled and got it to work...

 

 

Re: Eyedropper?

Gears Phenom Gears Phenom
Gears Phenom

Guys,

 

Does it work for imported body?

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Eyedropper?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I uploaded a new build. Hope it fixes it.

I saved my se file as x_t and read it back in.

The faces have colors but the macro will not see them.

There is no Style property on the faces anymore.

I don't know where it gets the color from.

LMGi
www.TLMGi.com

Re: Eyedropper?

Phenom
Phenom
When I import models that contains colors I always struggle to keep them.

I wonder where the face color are stored.

A great tool would be to get that colors and store them in facestyles

This is the macro that I would develop if I had more time.

Re: Eyedropper?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is probably a dumb question but how do you use it?

Attached is the list of files I end up with.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Eyedropper?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

See if this is enough to go by to get it running.

LMGi
www.TLMGi.com

Re: Eyedropper?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK, here's an example that illustrates a pet peeve. Why the heck are there still dialog boxes that are fixed in height and width so you can't see the full file names? Is this a DOS legacy or something.

So do I need both exes?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Eyedropper?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I must be doing something wrong. I have a part open and when I click the macro command a wheel spins for a couple of seconds and nothing. The prompt bar says "run macro" but when I move the cursor it reverts to the default "select geometry..." prompt.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Eyedropper?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
After you click the button it should display "Position mouse over face" in the prompt bar.
You can also run from Application button>Run Macro.
Make sure you have the zip ending in V2.zip
LMGi
www.TLMGi.com

Re: Eyedropper?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do have V2. Running from app button same thing. No joy. Restart SE or reboot?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200