Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FEMAP: two questions!

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

First question: should the FEMAP related questions be posted here on the Solid Edge forum or in the Simcenter forum? Or another place?

 

Second question: a FEMAP+NX Nastran customer states that only a user with Administrator rights can run FEMAP, or the following error occurs: "An error has occurred when trying to access the security device. Make sure it is properly installed and try again. (-2070)"

 

Customer already installed the latest dongle drivers but problem persists. I know that to install you must use an administrator account, but you also must be an administrator to run it?

 

Thanks.

1 REPLY

Re: FEMAP: two questions!

Siemens Legend Siemens Legend
Siemens Legend

Cadflow,

in the SImCenter Forum there is a sub forum for Femap, so I would recommend to post there.

 

https://community.plm.automation.siemens.com/t5/3D-Simulation-Femap-Forum/bd-p/Simcenter_3DFemap_for...

 

As far as I know the Admin permissions is only required during the installation. 

 

Regards /Ulf

Siemens EMEA GTAC Support