03-09-2017 05:48 AM
First question: should the FEMAP related questions be posted here on the Solid Edge forum or in the Simcenter forum? Or another place?
Second question: a FEMAP+NX Nastran customer states that only a user with Administrator rights can run FEMAP, or the following error occurs: "An error has occurred when trying to access the security device. Make sure it is properly installed and try again. (-2070)"
Customer already installed the latest dongle drivers but problem persists. I know that to install you must use an administrator account, but you also must be an administrator to run it?
Thanks.
03-09-2017 07:20 AM
Cadflow,
in the SImCenter Forum there is a sub forum for Femap, so I would recommend to post there.
As far as I know the Admin permissions is only required during the installation.
Regards /Ulf