Cancel
Showing results for 
Search instead for 
Did you mean: 

FLATTEN

Experimenter
Experimenter

Hello.

I have a problem with the attached piece. I´d like to flatten it but I have problems with the upper part. Please, could help me anyone?

Thanks in advanced

Mary

 

5 REPLIES

Betreff: FLATTEN

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


this only might work with a contour flange in traditional modeling not synchronous

 

regards

Wolfgang

 



regards
Wolfgang

Betreff: FLATTEN

Honored Contributor
Honored Contributor

The sheet metal flatten command will not work because the bend is not in a single axis.

 

What should work is using the surfacing type flatten command. The surfacing portion works from polygons rather than constant radius sheet metal bending. I can't help with using that as I have never used it, but I'm aware of that it can flatten complex geometry like this.

Betreff: FLATTEN

Legend
Legend

You might try changing to a part (file/switch to/part) to flatten. I use ST8, and have many parts that are not "traditional" sheetmetal parts, and I switch between part and sheetmetal to flatten.

ST8 MP9
Go FAST, or go home.

Re: FLATTEN

Experimenter
Experimenter

Thanks for your help.

I´m going to try.

Mary

Re: FLATTEN

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Mary,

 

This can be done with contour flanges - but you have to be in Ordered mode.

This video might help:-

(view in My Videos)

 

Cheers

Mark