Cancel
Showing results for 
Search instead for 
Did you mean: 

FOP Table - Cannot Save Settings

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

FOP Table Settings.pngFOP Table Properties

I created a custom Family of Parts Table and I want to save the settings.  But, as you can see from the above image, the option to name and save the settings is greyed out and not available.

 

Which text file does the FOP Table save to?

 

I narrowed it down to not being:

  • blocktable.txt
  • draftlist.txt
  • usertable.txt

 

And those are the only three text files I see to store table information.


____________________________________
--Scott Wertel, P.E.
5 REPLIES

Re: FOP Table - Cannot Save Settings

Gears Phenom Gears Phenom
Gears Phenom

@swertel  FWIW:  I just created a test case and see the same as you ST9 MP5

 

but to answer your question directly:  Heck if i know.

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: FOP Table - Cannot Save Settings

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Thanks for confirming, @Johnson_BigMatt.  I create IR 8893112.


____________________________________
--Scott Wertel, P.E.

Re: FOP Table - Cannot Save Settings

Siemens Phenom Siemens Phenom
Siemens Phenom
FYI, there are currently existing ERs requesting the ability to save the FOP table settings for reuse.

Re: FOP Table - Cannot Save Settings

Genius
Genius

Hello

I reported this in 2015 ( my IR 7516627), in answer i got this:

"This is working as designed. There is currently an existing ER requesting this functionality. I will attach this IR to the existing ER.
For whatever reason the product planner chose not have the functionality available with FOPs."

Smiley Frustrated

SE ST9 + TC 10.1.7

Re: FOP Table - Cannot Save Settings

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hopefully one more vote added to the ER gets it into the developers radar.  No reason that table functionality is not consistent across ALL tables, especially when the dialog is already there.


____________________________________
--Scott Wertel, P.E.