Fail to insert part from Part Library

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Something that very seldom happen and I dont know why.....

 

Failed to import part from Part Library in Solid Edge assembly.

 

After try to drag the part into the assembly, it failed and then suddenly hang ( cannot click any button)

 

Any of u experienced this issue before?

3 REPLIES

Re: Fail to insert part from Part Library

Esteemed Contributor
Esteemed Contributor

I can't answer your question but I notice you used a camera to record your actions in SE.

Do you have an icon in the lower right corner of your SE window like shown here:

videobutton.JPG

 

You can click it and record your SE session, save it, share it.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Fail to insert part from Part Library

Phenom
Phenom

In the Parts Library, try to rotate the model in the preview panel at the bottom using the middle mouse button or scroll wheel before dragging it into the assembly. After dropping the part, also Zoom Fit the view.

 

Also, does the part name show up in the Assembly tree ?

If yes, right-click the newly inserted part and select Show-Hide component and in the dialog,

 

2015093001.png

 

Then check ON Surfaces in the dialog that appears.

See if all this helps.

Re: Fail to insert part from Part Library

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Regarding the recording ICON, yes it's there...just the client didn't use it. I will ask client to use it later.

 

The issue is after bring the part into the assembly, the PC stop from working. Nothing can be click except the close window icon.

 

So I can not do right click to show/hide component in assembly.