Cancel
Showing results for 
Search instead for 
Did you mean: 

False drawings with automatic measurements, tolerances

Experimenter
Experimenter

Hello Edger,

 

since nearly 10 years I am a convinced SE User. But now I discovered an old big big mistake and nothing happens.

 

PRT: create an traditional model, add tolerances to the measurments

 

create an drawing, ovrtake the measuremnets automaticly

 

back to the model/PRT:

change the tolerance, store

 

DFT:

refresh the drawing, nothing happens, false toerance class

 

PRT:

change the measuremnet (eg 70 to 50), 

 

DFT:
refresh, the measuremnt change, the tolerance numbers changed, but the tolerance class is the same

 

So in this case SE produce since V17 false drawings. In 2008 I lost my job instead of false drawings. It was a company who produce hydraulic valve parts and the tolreance classes are very important

Instead of changing/refreshing the tolerance numbers, I thought all is OK.

 

Now I see that this mistake is still available and UGS means its an enhancement and no mistake!!! 

 

What can I do? I lost now my patience!! 

 

Thank you

 

Bernd

 

 

1 REPLY

Re: False drawings with automatic measurements, tolerances

Experimenter
Experimenter

Hi Edger,

 

nobody with an idea?

 

 

Noboldy with the same problems?

 

I tried to store the model under STP, relaod it as Sync model and make all measurement new ... with tolerances .... and the same

 

Is this noraml that I cant overtake the tolereances from the model?

 

What is my mistake?

 

Thanks

 

Bernd