Cancel
Showing results for 
Search instead for 
Did you mean: 

Family of parts members with different Subject field

Experimenter
Experimenter

Hi,

 

I would like to know if there is a way to make family part members with different Subject names. So far I found that if I write sth in Subject field (in  file properties) of Parent file I will get the same information in generated family member files which is not useful. 

I use Subject field in part lists so if I put two family members into assemly and than make a 2d draw with part list I will get two positions with the same name. 

So maybe anyone know if I can use some other field or add some variable or sth to put information like Subject name (different than part name/file name) into each FPM file from Parent file? 

It would be really helpful to be able to do it. eg. if I could use 'description' field in family part member table which unfortunately istn visible if its even present in FPM files at all.

So guys, any suggestions?

 

 

1 REPLY

Re: Family of parts members with different Subject field

Experimenter
Experimenter

OK ...

 

I found solution which was really easy but I didn't think about it at all.

After Populating Members and saving file in Property Manager there is an option to change the Subject field in each family part member separately.

 

Smiley Happy