Cancel
Showing results for 
Search instead for 
Did you mean: 

Fastener system error message ST8

Experimenter
Experimenter

Hi Everyone,

 

I have problem with fastener system.

while applying fastener to the angle surface it giving some error message .

e.g in case of two channel assembly.

i have attached the snap. 

fastening problem.jpg

 

 

 

Regards,

ST8 user 

vaibhav 

3 REPLIES 3

Re: Fastener system error message ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't use fastener systems but it seems apparent that with the angled face the implied axis is not normal to the face. Perhaps, if possible, select a different mate sequence without trying to align the angled face with the fastener face. Maybe using coaxial with connect or some such combination.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Fastener system error message ST8

Experimenter
Experimenter

Thanks for the reply.

I tried your solution. it is working only if one of face is flat.

what about both angled face?

Re: Fastener system error message ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Then that would mean the washers would not be normal to the bolt and nut. Therefore you'd have to use different mates. It can be done but, aside from model isssues, mechanically is it ok to have the bolt head and nut not normal to the washers or do you need beveled washers?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200