Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Fat lines in sketch environment!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @chrisstandring,

 

Woops, sorry. I re-read what I wrote, and corrected it.......as I still had to toggle the offending lines to/from construction, but I don't have a 2.5mm line width in the drop down selection.

 

2019-01-15 (1).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Fat lines in sketch environment!

Hi @chrisstandring,

 

To be able to change line width in sketch, first turn off "Relationship Color" on Inspect tab, Evaluate group.

Then, start line command, change the line width and finish line command.

Other line drawn will keep this setting of line width (even if you turn back on "Relationship color").

 

Hope that helps,

 

 

Michel Corriveau

Re: Fat lines in sketch environment!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yup, that did the trick here, thanks @Michel_Corriv.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Fat lines in sketch environment!

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

@Michel_Corriv, thanks for that.  I am very curious how the default changed to 2.5 mm on that one file, though!

Re: Fat lines in sketch environment!

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

@SeanCresswell, you have a 0.25 mm width in the drop-down list but not 2.5 mm.

Re: Fat lines in sketch environment!

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

We are not out of the woods yet.  After changing that default I was wondering why the point command was not working.  I then noticed that the points being placed were the same size as the "corrected" line thickness and as such, could not be seen if they were on a line.  Interestingly, the default point size is 2.5 mm, so that may or may not be a clue as to what is going on.

 

So changing the default line thickness also changes the default size of the points.  Now the lines are behaving but I have to make every single point larger!  I am going to send this one in to GTAC!

Re: Fat lines in sketch environment!

Hi @chrisstandring,

 

I can't reproduce your problem.

Point size is staying at 2.5mm regardless of line width.

 

I'm on SE 2019 MP 04 ...

 

 

Michel

Re: Fat lines in sketch environment!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Michel_Corriv wrote:

Hi @chrisstandring,

 

I can't reproduce your problem.

Point size is staying at 2.5mm regardless of line width.

I'm on SE 2019 MP 04 ...

 

Michel


Same here.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Fat lines in sketch environment!

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

@Michel_Corriv@bshand, to reproduce the problem please open the attached part file and follow the nine steps illustrated in the nine attached pictures Step 1 to Step 9 inclusive.  Let me know if I have screwed up somewhere and how to fix it.

 

Cheers,

 

Chris

Re: Fat lines in sketch environment!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not sure what's going on yet but I did spend a few minutes. Once I got the lines and points to insert independently, closed the part, then couldn't repeat that.

I opened a new ansi inch default template part and there was no issue with "cross contamination". Also with the default template the point has a 2.5mm width whereas line has a 2.0mm max width.

I didn't spend a lot of time with it but I'd say, just to put it to bed, so I can go to bed, that part has an anomaly of some kind.

Bottom line I don't think it's a general code design fault.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200