Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Missing From ST10

Creator
Creator

On ST9 there was a feature that when you did a "Save As" the dialog box would pop up with text boxes where you could change the document number and the revision number. That was a very handy feature that I used a lot. Was it removed from ST10?

5 REPLIES

Re: Feature Missing From ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Metalbutcher  It is there in ST10 but is part of the Built in Data Management (BiDM).  It is most likely turned off and you need to turn it on.  Can do that in your Options on the  Manage section.

2018-03-14_14-37-27.png



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Feature Missing From ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Metalbutcher,

 

Pretty sure I know what part you are refering to.......and I think, if you go to Solid Edge Options, on the Manage tab, you need to check the box "Use Solid Edge data management"......and those "very handy" [indeed] fields will be restored.

 

 

 

2018-03-15 (1).png

 

2018-03-15 (2).png

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Feature Missing From ST10

Creator
Creator

Thanks guys. That's exactly what I needed.

Re: Feature Missing From ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Metalbutcher

 

 

 

but the only difference to ST9 will be, taht aslong as You have not turned on the forcing of using documentnumber and revision number as file name, those fields only will be used for doc properties rather than filename.

 

But if turn this option on, the common proeprty dialog will appear when saving

 

 

regards
Wolfgang

Re: Feature Missing From ST10

Creator
Creator

Yup, and that's fine with me. Smiley Happy