Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Feature Name callout in hole table ST6

Experimenter
Experimenter

Hi 

I would like to add hole feature name in hole table, which is I have renamed in 3D model hole feature that should be reflect in hole table when drafting. kindly suggest me how to add this one into hole table

 

Thanks

saravanan ponnusamy

1 REPLY 1

Betreff: Feature Name callout in hole table ST6

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Ponnusamy

 

 

I don't think that this will be possible.

The feature name is no property which can be  read out from the 3D file directly.

All gemetric values, dimters, etc. will be possible values for getting automatically.

Names are not common used for use as draft info.

 

regards
Wolfgang