Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature call out quantity.

Valued Contributor
Valued Contributor

I've created a feature call out for hole call outs, it works fine for holes where there are more than 1 of the same hole. But i would like it to not show 1 x for a hole where there is only one instance.

 

the call out code is %QC x %DI%HS %HC THRU

 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
19 REPLIES 19

Re: Feature call out quantity.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Smart Quantity is what you want.

Maybe this post will help.

LMGi
www.TLMGi.com

Re: Feature call out quantity.

Valued Contributor
Valued Contributor

Thanks, can you confirm what i need to do get what im after please

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Feature call out quantity.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Put %QN in the feature callout tab Simple Hole space. Put "%QC x" in the smart depth tab Hole Quantity Note space.

 

Check out this help topic:

https://docs.plm.automation.siemens.com/tdoc/se/110/se_help/#uid:calout4h

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Feature call out quantity.

Gears Phenom Gears Phenom
Gears Phenom

Go into your dimension style, go to the "Smart Depth" tab. In hole Quantity Note, enter in %QC and whatever you want displayed with the count (9 X, 9 PLCS, etc.), then go into the "feature Callout" Tab, under the field "Simple" enter in %QN. This will do as you wish.

SMART QUANT.JPGSMART QUANT2.JPG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Feature call out quantity.

Valued Contributor
Valued Contributor

Thanks All!

 

@nominus38 I copied what you put and it sorts the smart quantity issue i was having, but one more thing  that isnt working is getting the word THRU next to a through hole callout. 

In the smart depth tab the hole depth through has been set to THRU. (where yours shows blank)

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Feature call out quantity.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

but what is Your questionnow?

 

If You put the text "THRU" into a through  hole then SE will write this text as smart depth text info to a hole feature.

 

Therefore there - by default - is nothing for a through hole.

Normally no depth info is needed there, isn't it?

 

 

regards
Wolfgang

Re: Feature call out quantity.

Valued Contributor
Valued Contributor

@hawcad

 

i have the word THRU in the tab shown but the call out isnt picking it up.

 

i would like any through holes to show the word THRU and any Finite holes with a defined depth to be shown as <DepthValue> DP  

 

 Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Feature call out quantity.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

I just see that my last answer was dropped by the forum - an error message appeared, that there are service changes.

 

So can You upload a small example with the draft and the part file to see, why and how?

 

 

regards
Wolfgang
Highlighted

Re: Feature call out quantity.

Legend
Legend

In any manufacturing, is it normal to state every hole as through? I have only seen otherwise shown, with the specific depth required, if not through. My experience is mostly sheet metal, and some machining, so this request is odd to me. But, I'm happy to learn something new!