Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature call out with count

Experimenter
Experimenter

Hello everyone,

 

please kindly inform me how to make feature call out with count.

 

for your reference the Conterbores in red are the same size.

also the lower smaller holes are same thread.

is there any tool in solid edge to detect automatically in feature call out? or i need to use suffix manually

Feature callout.JPG

3 REPLIES 3

Re: Feature call out with count

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

This will be new in Solid Edge ST9! Smiley Wink

 

link

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Feature call out with count

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


maybe in the meantime  a hole table can help a little.

 

It will show at least the holes together with a counting number,
so you can see where and how often a hole is there.

 

 

regards
Wolfgang

Re: Feature call out with count

Experimenter
Experimenter

Helo everone,

 

thank you for the answer, so i will be wait for ST9 Smiley Tongue