Feature request: ability to choose peervariables to change with goalseek

Experimenter
Experimenter

for example: if i want to get the centre or mass in the middle i have to draw a contraweigt inside the part file and then use goalseek to get the centre of mass in the middle, the contraweigt should be another part in an assembly but then i can't choose peer variables to get it to change with goalseek. so i draw it as 1 part but it should be 2 parts.Part1.jpg

 

Part3.jpg

2 REPLIES

Re: Feature request: ability to choose peervariables to change with goalseek

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

How about making the part as a multi-body? When solved you can then "publish" the individual parts.

 

The Add Body command Capture3.JPGis on the Home tab→Solids group in both ordered and synchronous environments.

A new part or sheet metal file contains a single design body. In a file with a single design body, the Design Bodies collector does not appear in PathFinder. If you want to use the multi-body modeling method, use the Add Body command to create a multi-body file.

You can use the Add Body command in a new file to assign a name to the initial design body. The default name for the initial solid body is Design Body_1. As you add solid bodies to a file, the Add Body dialog box contains the active design body name.

 

Cheers

Mark

Re: Feature request: ability to choose peervariables to change with goalseek

Experimenter
Experimenter

thank you for your answer,

 

i will try this but sometimes the asm is more complicated, i chose the easiest example.

 

this means i will have to design it with multiple bodies then pubish it and assemble it in asm again, could take alot of time.