Cancel
Showing results for 
Search instead for 
Did you mean: 

File extensions

Experimenter
Experimenter

Hi, when I save my draft files, the file extension used to be .dft.  Now however, it is either .psm.dft or .asm.dft. It keeps the original file extension and just adds the .dft behind it. How do I stop it from doing this?

4 REPLIES

Re: File extensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hey Vaughn,

 

This is a known issue with MP2 on ST7......and a fix is slated to be underway.

The immediate fix is to roll-back [if it were only that easy] to MP1.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: File extensions

Honored Contributor
Honored Contributor

I was about to from MP0 to MP2, glad I did not.

Re: File extensions

Gears Phenom Gears Phenom
Gears Phenom

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/ST7-MP2-source-extention-in-dft-file...

 

PR 8253794

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: File extensions

Phenom
Phenom

Just had this happen to me... thought I just was just having another bad day!

 

Glad to know it's in the works.