Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: File name and custom property in same column of part list

Valued Contributor
Valued Contributor
Hello @bshand,

Please note that, I/we don't use connect type as bolt/part name. And that is not my intention. The property will only be used for easy bolt count, and it will be hidden in BOM. As I said, it is already explained before in detail. Sorry for confusion.

Thank you for your reply.

Regards,
Aslam
Highlighted

Betreff: File name and custom property in same column of part list

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@aslam, OK. Since I'm obviously not understanding I'll avoid further responses on this thread.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: File name and custom property in same column of part list

Gears Phenom Gears Phenom
Gears Phenom

@aslam  That is what I meant. Can you not have the bolts, nuts, what-have-you simply have the description as it's filename? This is what I do, and it works fine for me. Sure, you can't use some symbols like for fractions (i.e. "1/4-20 UNC HEX BOLT" must be named a different way, either like .25-20 UNC or 1_4-20) but it works. And it seems that it would satisfy all of what you're needing, except no idea why the "connection type" is going to matter but to each his own I guess.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: File name and custom property in same column of part list

Valued Contributor
Valued Contributor

BOLT PART LIST.JPGHello @bshand@nominus38

 

It seems that I have made so many confusions. Extremely sorry for that.

That's why I have attached an example image for easy visualization of the issue.

 

The left part list is actual part list which we use, and it must be like this.

The right one is expected breakdown. The grouped by type column is which I was talking about.

I have to make the right side table manually in excel always to count bolts in a project clearly.

 

If the TYPE column can be added in the part list while checking, that will be good enough. After that I will hide the column before printing.

 

Regards,

Aslam

Betreff: File name and custom property in same column of part list

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @aslam

 

 

 

as already said, this exactly is whatfor the Occurency Properties(OCP)  now are used.

Give them as needed to an OCP and use them as group item in BOM

 

regards
Wolfgang

Betreff: File name and custom property in same column of part list

Valued Contributor
Valued Contributor
Thank you again @hawcad for your reply.

I will try that when enter to ST10.
Thanks.

Regards,
Aslam

Betreff: File name and custom property in same column of part list

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @aslam

Hi @bshand

 

 

 

I have to apologize for my answers here.

Just seen - thanks again to @bshand and his PM, that You can use Occurency Proeprties for be shown in the BOM, but SE does not split them accordingly.

So You only see those properties, but YOu will not get out a count with that methode.

 

See following picture and the CallOut texts with different OCP and the entries in the BOM, but as said, sorry for that, no quantites.

 

20180404_2021.PNG

 

So this has lead me into a wrong direction.

Sorry for sending You to that direction too!

 

regards
Wolfgang

Betreff: File name and custom property in same column of part list

Valued Contributor
Valued Contributor
Hello @bshand,
Thank you for your action. The approach is very appreciated and professional.

Hello @hawcad,
Thank you very much for the detail workout and expressing the whole matter with full transparency. The way you and bshand responded together, I call it 'Professional Honor' and 'Professional Honesty! I salute you both!

Hopefully we will find solution soon.

Thank you again, both!

Regards,
Aslam