Cancel
Showing results for 
Search instead for 
Did you mean: 

File size of SE_SharePoint_Server_MP2?

Good morning everyone,

 

The size of the maintenance pack for SESP is normally around 190MB. I have noticed that the size of MP2 is now 1.48GB and it is largely because of a V106 file. Please see the screenshots below. Can someone please confirm if this is correct? In South Africa we regard bandwidth as a precious commodity.

 

Kind regards,

Theodore

 

Capture_02.JPGCapture_01.JPG

 

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3
1 REPLY 1

Re: File size of SE_SharePoint_Server_MP2?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I saw that in there also and was wondering why it was there...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com