Cancel
Showing results for 
Search instead for 
Did you mean: 

Files generated by the Solid Edge

Pioneer
Pioneer

Hi All,

 

could you please to tell me what types of files are been generating by Solid Edge during creating the parts and assemblies.

 

I am facing the problems with the links and have missing links in my assemblies. ( not every file is missing ).

 

Thank you,

 

Arek

Solid Edge ST8 MP10
2 REPLIES 2

Re: Files generated by the Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Solid Edge generates files with the following extensions:

  • PAR - Parts
  • PSM - Sheet Metal
  • ASM - Assembly
    • CFG - Assembly configurations (does not affect links if missing)
  • DFT - Draft


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Files generated by the Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @ArekK,

 

If you are getting missing links in your assembly, this is more likely that the files that were there, are now been either relocated or renamed within your filing system.

There are a few tools within Solid Edge to help repair this....suggest reading the help file on the "Missing Links" & "Replace Part" topics, for more.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000